最近在做一个交流有效值转换的东西,用到了ad637,电路是按照datasheet上的标准RMS连接做的。CAV取得是10uF。BUFFIN、COMMON、OUTPUT OFFSET接地。用信号发生器产生一个频率为200K峰峰值为2V的正选信号,经过AD637后,用万用表直接测量AD637的输出端为0.685V,跟理论的0.707V相差比较大,并且测量数据不稳定,相同的条件下再次测量变为0.662V,数据还一直变动,有时是0.702V。想问下这是怎么回事,请高手赐教。
建议你试一下数据手册中图8或图11的电路。在数据手册中介绍了一些关于Trim的方法。还有就是电容值的计算。你可以根据那个算一下你选的Cav是否合适。