已回答假定已回答

咨询旋变数字转换器AD2S80A手册问题

徐晓伟 在 2015-5-25 詢問的問題
最後回覆由nandin於2015-5-28提供

       你好,在使用贵公司的旋变数字转换器AD2S80A时遇到旋变输出信号与参考信号相移问题,查询手册发现疑问,请求解答和帮助。              先说一下现象:        

       我使用的位置传感器为双通道的正余弦旋转变压器,指标为:励磁为2KHz,4Vrms,粗机和精机变比为1:16,轴转速为1°/s,实际测试过程中发现参考信号(对应手册中“REFERENCE I/P”,在R3和C3滤波之前的信号)与粗机的信号之间相移为5°,但与精机的信号之间相移为25°。想确认一下对解算精度是否有影响。       

       查询手册发现有几个地方对我们使用造成误解,请明确说明:       

        1、官方手册P5页的“RECOMMENDED OPERATING CONDITIONS”中的“Phase Shift Between Signal and Reference . . . ±10 Degrees (max)”,这里是不是指的就是AD2S80A芯片的SIN或者COS信号与参考信号(对应手册中“REFERENCE I/P”,在R3和C3滤波之前的信号)之间的相位差,如果不是请说明具体指的是什么。如果是,我觉得与P13页中的“Differential Phase Shift”说明有冲突,这里面说明的附加误差是否和这个±10°有关系,从你手册中举例来看到:“ For example, for a phase shift of 20 degrees, a shaft rotation of 22 rps and a reference frequency of 5 kHz, the converter will exhibit an additional error of:”(手册原文)       

       上述已经说明了相移之间的误差是20°,这个上述你说明的“Phase Shift Between Signal and Reference . . . ±10 Degrees (max)“已经违背了,怎么还能通过调整相移来改变影响了,希望给予解答。       

        2、官方手册P8页的”5. Closed-Loop Bandwidth Selection (C4, C5, R5)“中”ensuring that the ratio of reference frequency to bandwidth does not exceed the following guidelines“,这里说明了基准频率和带宽之间变比是”不超过以下建议的标准“,但我从你们官方下载数设计工具中确实建议这个基准频率和带宽之间的变比是”不小于以下建议的标准“,而且我看你手册中的举例,P14的典型电路”TYPICAL CIRCUIT CONFIGURATION“中也写明了”a reference frequency of 5 kHz and a maximum tracking rate of 260 rps with a bandwidth of 520 Hz“,这里基准频率是5000Hz,带宽是520Hz,用的是12位解算方式,比例应该是9.6:1,已经超过了建议的标准4:1。这里请确认你手册是否正确,我觉得应该是”不小于“。     

        针对上述两个问题希望贵公司尽快给予我解答,我主要关心的是旋变的参考信号与精机的信号之间相移为25°是否超过了你们要求的相移偏差大小,超过了对精度是否影响,应该如何进行修改。

結果