已回答假定已回答

问题: 怎么使用ADI MPEG-4 SP/ASP Encoder library??

Run 在 2012-12-25 詢問的問題
最後回覆由wangmigooo於2013-1-13提供

ADI官网提供的mpeg4编码库libmpeg4enc_BF561_48.dlb,根据指导手册上说的写了源代码,但是在编译的时候出现下面的问题,使用的是默认的ldf,未修改。是否用修改ldf呢?怎么修改呢?

 

[Warning
li2060] The following input section(s) that contain program code
and/or data
have not been placed into the executable for processor 'p0'
as there are no
relevant commands specified in the
LDF:

 

.\libmpeg4enc_BF561_48.dlb[mpeg4_enc_13.doj](adi_fast_prio5_code)
.\libmpeg4enc_BF561_48.dlb[mpeg4_enc_13.doj](adi_fast_prio6_code)
.\libmpeg4enc_BF561_48.dlb[mpeg4_enc_13.doj](adi_slow_noprio_code)

 


[Error
li1060] The following symbols are referenced, but not
mapped:
'_ADIMPEG4ECodecNew0ea93040ed02d78b4ad7eb6b4b36a7be' referenced from
corea.dlb[mpeg4enc.doj](program)

 

Linker finished with 1 error and 1
warning
cc3089: fatal error: Link failed

 

使用的是vdsp5.0 up9
。如果要修改ldf是不是得学他的语法啊?还有 库一般怎么调用啊?小弟初来乍到,忘大家指点:)

結果