已回答假定已回答

有关ADuCM360 / ADuCM361的ADC1内部通道的问题请教!

lpc_2138@126.com 在 2015-11-5 詢問的問題
最後回覆由ADI_XUN於2015-11-13提供

项目中,在验证ADuCM361的ADC1内部通道AVDD/4时,按照Hardware User Guide第30页中的设置方法:

The AVDD/4 settings are as follows: ·

Select DAC as AIN and set the DAC output to 600 mV ·

·pADI_DAC->DACCON = 0x410 ·

·pADI_ADC1->DAT = 0x8000000 (此处应该配置DAC的值:pADI_DAC->DACDAT = 0x8000000;)

·pADI_ADC1->CON = 0xBC1AC (二进制补码双极性,内部参考1.2V,AIN+=AVDD/4,AIN-=DAC)

·pADI_ADC1->MDE = 0x1 (PGA gain=1,连续转换模式)

·AVDD supply = (ADC voltage + DAC) × 4

 

    读取ADC1的ADC1DAT寄存器,得到 0xFFAD5240,VADC=0xFAD524/(2^24)*1.2V-1.2V = -0.024V,

得到AVDD=(-0.024V+0.6V)*4=2.3V,而电路中AVDD的实际电压是3.3V。请问:得到0xFFAD5240这个数据对吗?

计算方法和配置有没有问题?

結果