已回答假定已回答

如何理解AD7746的电容寄存器里的二进制数

tongguowei18 在 2016-4-13 詢問的問題
最後回覆由wangmigooo於2016-4-14提供

AD7746的说明书中有这么一段

The 0x000000 code represents negative full scale (–4.096 pF),
the 0x800000 code represents zero scale (0 pF), and the
0xFFFFFF code represents positive full scale (+4.096 pF).


我参考了数据表格后,发现电容的数据被分到了三个寄存器中,地址分别为0x01 0x02 0x03


我的理解是当把这三个寄存器的值取出后,(假设ADC设置为4pF,其他不变)那么电容的结果应该是

图片1.png


这三个寄存器的二进制数首尾相连组成的数字占8pF的比例?

 

結果