已回答假定已回答

ADF5355输出频率设置问题

yanhao 在 2016-7-23 詢問的問題
最後回覆由Benz於2016-8-10提供

1、用10MHz做ADF5355频率输入,要得到输出频率11.3GHz是否可以?但是按照手册里所讲的,要得到些频率输出好像是不需要参考输入信号的,是不是?

 

2、如果是要参考10MHz输入,按照数据手册34页所给的公式,因为集成VCO频率范围是3.4G~6.8G,要得到11.3G需要倍频,取VCOout=11.3GHz/2=5.65GHz,Fpfd=10MHz/2=5MHz,最后计算得到只设置INT=VCOout/Fpfd=5.65*1000/5=1130即可,因为通过计算得出FRAC=0,此计算是否正确?输出是从RFOUTB输出的,如下图标示处1?

 

3、按照34页所给的例子中计算不部有些不懂:

3.1、里面所述“In this example, the 122.88 MHz reference signal is divided by 2 to generate fPFD of 61.44 MHz. The  esired channel spacing is 200 kHz.”,其中这200KHz是怎么来的?

3.2、在计算过程中MOD2=(61.44MHz/GCD(61.44MHz,200KHz)=1536,这个是如何计算的?

3.3、因所要输出的频率为2112.8MHz,在VCO之外,所能VCO=RFout*2=4225.6MHz,从RFoutA输出,是否,如下图标示处2?

 

ADF5355.PNG

結果