已回答假定已回答

Aduc7023评估板  无法下载程序

Edward_Shao 在 2016-10-27 詢問的問題
最後回覆由Edward_Shao於2016-11-2提供

评估版型号为EVAL-ADUC7023QSPZ,开发环境为keil,并且按照光盘中的文档一步步进行设置,基本的设置都没问题。

当进行到Debug步骤时,Jlink无法下载程序显示下面的错误信息:

Trying to connect with 5 kHz !

Info: ADI system TAP: Connecting to device with system TAP.

Info: TotalIRLen = 5, IRPrint = 0x01

Info: Analog devices system TAP: Enabling CPU core.

***JLink Error: ADI system TAP: Could not read CPU core Id.

Invalid core Id. (0x00000000)

请问这个问题如何解决呢?谢谢各位!

結果