已回答假定已回答

关于adxl03灵敏度的问题

wangyc 在 2017-3-26 詢問的問題
最後回覆由neilzhao於2017-4-12提供

ADXL103的灵敏度问题,我看到以前提的问题:

Q1:“The ADXL103/ADXL203 output is ratiometric, so the output sensitivity (or scale factor) varies proportionally to the supply voltage. At VS = 3 V, the output sensitivity is typically 560 mV/g. Sensitivity at XOUT, YOUT VS = 5 V is 1000mv ”  ,说明书上这两处,似乎有误,如果5 V Sensitivity是1000mv,3 V Sensitivity应该是600mv。

 

A1:VS=3V时,灵敏度是560 mV/g。灵敏度随供电的变化是线性的。5V供电灵敏度是1000mV/g。其他供电下的灵敏度使用根据这两个点根据线性计算

Q2:按以上说法 那电压为0的时候 灵敏度为-100mv/g,明显不正确,没有电压了怎么可能有输出呢。而且说明书第三页有 “Sensitivity is essentially ratiometric to VS. For VS= 4.75 V to 5.25 V, sensitivity is 186 mV/V/gto 215 mV/V/g.”不符合3伏和5伏的线性关系

----我想知道最后的结果?我现在用的是3.3v电源,按3-5V的线性关系计算结果是:560+(3.3-3)/(5-3)*440=626MV/g。是这个数吗?

为什么电源在4.75v是,186MV/V/g ,则186*4.75=883.5MV/g,这个值并不符合比例关系。按比例关系算应该是

560+(4.75-3)/(5-3)*440=945MV/g,

到底怎么算?

結果