已回答假定已回答

在项目中遇到关于AD9288的一些疑问,请ADI专家帮忙解答 谢谢

cherryljl 在 2013-1-17 詢問的問題
最後回覆由wangmigooo於2013-1-17提供

我们在一个低端DSO的项目中,需要用到AD9288,在较仔细阅读AD9288的datasheet后,任有以下疑问,麻烦ADI的专家帮忙解答。谢谢。
1.AD9288输入信号的范围是否为 1Vpp+0.3*VD ,即在VDD为3.3V时,输入信号的范围为+0.49V~+1.99V?
2.在AD9288的评估板中,采用的是变压器耦合的方式,如果用全差放AD8138来驱动AD9288,可否将EVM中的C30和C39两个隔直电容去掉,因为我们需要测量输入信号的直流分量。
3.在EVM中AD8138的Vcom引脚的驱动电压取自电源分压,由于考虑到实际项目中电源不可能很干净,Vcom直接取自电源可能不太妥当,能否将AD9288第6脚的参考电压经分压后驱动Vcon?第6脚是否有足够的驱动能力?
4.在datasheet的第14页关于数据有效的描述如下:“In other words, if two clocks are fed to the AD9288 and are 180° out of phase, enabling the data align allows Channel B output data to be available at the rising edge of Clock A.”但是在第5页和第6页的时序图中显示,数据是在时钟的下降沿有效,请问哪种理解正确?
麻烦ADI的专家解答,感谢.

結果