已回答假定已回答

关于ADV7842的CVBS采集

Strachey 在 2017-7-18 詢問的問題
最後回覆由FAUSTON於2017-8-17提供

@adi_angela

 

Dear all,

       我在调试ADV7842采集CVBS的时候遇到一点问题,恳请大家给点指导,谢谢!

       下面是我的配置,当采集NTSC的时候,图像很正常,但当视频源改为PAL的时候,过一段时间就同步不上,就会整屏幕跳动闪烁,过10多分钟又可以同步上,然后过一段时间又同步不上,如此循环。

        当40 06 26寄存器改为40 06 A6时(实际应该是使用vs信号而不应该是field信号),NTSC和PAL都能同步上,整幅画面都不会大范围跳动,但是图像质量很差,会小范围跳动。用示波器查看VS/Field、HS、DE信号时,波形正常无串扰。7842后端需要采用逐行方式采集,但应该由于I转P导致帧率翻倍了。不知道是否是由于I转P导致的现象?请问我现在该如何调试?谢谢!

 

Best regards!

 

配置如下:

#i2c reset

40 FF 80 # I2C reset

 

#i2c address set

40 F1 90 # SDP map

40 F2 94 # SDPIO map

40 F3 84 # AVLINK

40 F4 80 # CEC

40 F5 7C # INFOFRAME

40 F8 4C # AFE

40 F9 64 # KSV

40 FA 6C # EDID

40 FB 68 # HDMI

40 FD 44 # CP

40 FE 48 # VDP

 

#IO

40 00 01 # CVBS 4x1 mode

40 01 00 # SD core

40 03 80 #* 16 bit 422 mode

40 04 62 # Output bus rotation (default)

40 06 26

40 0C 40 # Power up Core

40 15 80 # Power up pads

40 19 C3 # LLC DLL phase

40 33 40 # LLC DLL enable

 

#AFE

4C 0C 1F # ADI recommended write

4C 12 63 # ADI recommended write

4C 00 0E # ADC0 power Up

4C 02 80 # Manual Mux

4C 03 B0 # Ain11

 

#SDPIO

94 7A A5 # Timing Adjustment

94 7B 8F # Timing Adjustment

94 60 01 # SDRAM reset

94 97 00 # Hsync width Adjustment

94 B2 60 # Disable AV codes

 

#SDP

90 00 7F # Autodetect PAL NTSC SECAM

90 01 00 # Pedestal Off

90 03 E4 # Manual VCR Gain Luma 0x40B

90 04 0B # Manual Luma setting

90 05 C3 # Manual Chroma setting 0x3FE

90 06 FE # Manual Chroma setting

90 12 09 #* Frame TBC off,3D comb,IP enabled

90 A7 00 # ADI Recommended Write

附件

結果