已回答假定已回答

有关AD7124-4的编程问题

jingwang_870 在 2018-3-14 詢問的問題
最後回覆由EmmaChen於2018-4-20提供

AD7124-4的错误寄存器,读的数据是0X00,0X00,0X40,手册上:

When a CRC check of the internal registers is being performed, the on-chip registers cannot be
accessed. User write instructions are ignored by the ADC. Set this bit so that the SPI_IGNORE_ERR
bit in the error register informs the user when write operations must not be performed.

 

我的理解是:当对内部寄存器进行CRC检查时,不能写入on-chip寄存器。用户指令被ADC忽略。当寄存器的CRC检查发生时,就设置这个位。的当检查完成时,位被清除;写操作只能在那时执行。这种情况下,软件应该怎样处理?请高手解答一下谢谢

結果