已回答假定已回答

关于AD9963芯片没有输出的一点问题

bzqian 在 2014-2-17 詢問的問題
最後回覆由adi_yu於2014-2-24提供

您好,我在研发过程中,使用AD9963芯片,在XILINXEDK开发工具中利用SDK对其进行配置,配置情况如下:

* Default AD9963 configuration:
-Full-duplex mode (Tx data on TXD port, Rx data on TRXD port)
-Power up everything except:
-DAC12A, DAC12B, AUXADC (all unconnected on PCB)
-DLL
-Clocking:
-DLL disabled
-ADC clock = DAC clock = ext clock (nominally 80MHz)
-Tx path:
-Data in 2's complement (NOTE: datasheet bug!)
-TXCLK is input at TXD sample rate
-TXD is DDR, I/Q interleaved, I first
-Tx interpolation filters bypassed
-Tx gains:
-Linear gain set to 100%
-Linear-in-dB gain set to -3dB
-DAC RSET set to 100%
-Tx DCO DACs:
-Enabled, configured for [0,+2]v range
-Set to mid-scale output (approx equal to common mode voltage of I/Q diff pairs)
-Rx path:
-TRXCLK is output at TRXD sample rate
-TRXD is DDR, I/Q interleaved, I first
-Decimation filter bypassed
-RXCML output enabled (used by ADC driver diff amp)
-ADC common mode buffer off (required for DC coupled inputs)
-Rx I path negated digitally (to match swap of p/n traces on PCB)
*/

 

通过读取AD9963的寄存器的可以验证其寄存器都已经正确配置了。用示波器观察信号,测得时钟频率正确,DAC的TXD port有信号输入,但是DAC一直没有信号输出。

 

请问可能是什么原因造成这种现象的呢?有什么排查的方法吗?

 

望各位大神指教。。。。。。

結果