已回答假定已回答

21375里面不能使用sigmastudio吗?

liangbread 在 2014-3-22 詢問的問題
最後回覆由Sue.Wu於2014-3-26提供

我准备在21375中使用sigmastudio,但是在我修改ldf,分配好sigmastudio里面所需要的10个memory block之后,调用sigmastudio动态库里面的adi_ss_comm_init()等函数的时候,CCES在编译之后报错,说只支持2136x,具体如下:

[Error li1150]  The following input file(s) machine specification is incompatible with 'ADSP-21375':

    libadi_sigma_sharc_nwc.dlb[adi_ss_sharc_communication.doj] (ADSP-2136x)

    libadi_sigma_sharc_nwc.dlb[adi_ss_init_asm.doj] (ADSP-2136x)

 

 

Linker finished with 1 error

cc3089: fatal error: Link failed

make: *** [processor-21375-CCES.dxe] Error 1

这个问题是可以通过修改编译器里面定义的processor为2136x可以解决的吗?还是说无法解决?

結果