已回答假定已回答

请教文件包括问题

ty228 在 2014-4-12 詢問的問題
最後回覆由liangbread於2014-4-13提供

在VDSP++5.0的工程里文件夹里放入test.h文件,在工程的某C文件里include"test.h" ,编译通过,然后把test.h文件改名为test2.h,C文件里的include"test.h"改为include"test2.h" ,编译通不过了,出现了:

----------------Configuration: 21479 AD1939 C Sampled-Based Talkthru 48 or 96 kHz - Debug----------------
C:\Program Files\Analog Devices\VisualDSP 5.0\gmake-378: *** No rule to make target `test.h', needed by `Debug/process_audio.doj'.  Stop.
No valid command(s) to build.
Build was unsuccessful.

 

请教是什么原因及怎么解决?谢谢!

結果