已回答假定已回答

如何实现多片AD9361射频同步?

tju_kai 在 2014-12-14 詢問的問題
最後回覆由ADI_Wei於2014-12-17提供

您好!在AD-FMCOMMS5-EBZ开发板上有两片AD9361,我一直没找到关于射频同步的相关资料,UG-570只有基带同步的说明,所以不理解开发板上是如何实现RF同步的。在“http://www.analog.com/en/evaluation/eval-ad-fmcomms5-ebz/eb.html”中提到“The AD-FMCOMMS5-EBZ also contains dual ADG918 SPDT switches, which create a calibration matrix between the two AD9361s. This switch matrix hardware, combined with the Analog Devices supplied API software, allow for a full digital and RF synchronization between the two AD9361s.”这句话的意思好像是说通过单刀双掷开关芯片ADG918可以实现RF同步,实在不明白其中的原理。另外,在AD-FMCOMMS5-EBZ开发板的原理图中我发现两片AD9361都使用了同源的外部LO,是不是因为这个设计才实现射频同步的?总之,就是如何实现多片AD9361的RF同步,包括硬件如何连接和软件如何配置?(我想实现4片AD9361的射频同步)

結果